How to search for all b3 analog inputs that are Out of Service.

Issue

Need a quick way to find all the analog inputs under all the b3s in the system that are out of service.

Product Line

SmartStruxure Solution

Environment

Workstation

Enterprise Server

Automation Server

b3s

Cause

Documentation

Resolution

  1. Create a Search object at the ES or AS level and configure as follows...


     
  2. In this example the search object is in the ES and it will search for b3 inputs in all of the Automation Servers under the ES.

 

The search can easily be modified to search for other types of objects that are out of service by changing the class filter.