DigitalSentry software upgrade installation fails to install on a DSSRV.


Unable to complete the Installation for Digital Sentry. 

Product Line

Pelco Video Management


  • DSSRV Series


Not enough free disk space on C:\ drive because Temp Folder on the DSSRV is occupying over 21GB space


Run Disk Cleaner

  1. Click on the Start Menu.
  2. In the search box, type Disk C and then click the [Enter] key.
  3. Select Disk cleanup.
  4. Verify the total amount of disk space taken.
  5. Click the OK button.
  6. Click the Delete button to delete the files.
  7. Verify Disk C:\ drive now has more free space