How do I wire multiple PTZ cameras to the DX3100 Series DVR

NOTICE

DISCONTINUED PELCO PRODUCT.
This product has been discontinued. For further information please visit pelco.com/support/discontinued-products

Issue

How do I wire multiple PTZ cameras to the DX3100 Series DVR

Product Line

Pelco Video Management

Environment

  • DX3100 Series DVR
  • PV140
  • CM9760-CDU-T

Cause

  • Installation

Resolution

There are two methods for wiring PTZ cameras to the DX3100: Home run or Daisy chain.

Daisy Chain using the PV140

Homerun  using the PV140 and the CM9760-CDU-T