Connecting an external device to a USB port on DX4100.

Issue

USB mouse is not working

Product Line

Pelco Video Management

Environment

  • DX4100 Series

Cause

USB mouse not supported.

Resolution

USB 2.0 Port: Connects USB storage devices.  The High speed USB port is located under the rubber cover.

NOTE:

  • Do NOT install a USB style mouse device to the DX4100.
  • Two additional high speed USB ports are located on the rear panel.