How to connect IR850S-65/IR940S-30 Infrared LED Illuminators to Esprit HD camera

Issue

Connecting IR850S-65/IR940S-30 Infrared LED Illuminators to Esprit HD camera

Product Line

Other, Pelco Cameras

Environment

  • IR850S-65/IR940S-30 Infrared LED Illuminators 
  • Esprit HD Series ES5230
     

Cause

Connecting IR850S-65 Infrared LED Illuminators to Esprit HD camera

Resolution

IR850S-65/IR940S-30 Infrared LED Illuminators

1. Black AC/DC- and Red AC/DC+ power wires

Note: Leave Orange and Purple wires shorted together for Telemetry input and White and Yellow wires for Photocell Following Contact

 

 

 Esprit HD ES5230 Series camera

1. Open the Esprit's enclosure and connect the Black AC/DC-  and Red AC/DC+ power wires to TB2 and TB3 terminals as pictures showed below: