How to use the HTML5 Viewer in SmartStruxure WebStation

Issue

How to enable and use the HTML5 Viewer instead of the Java Viewer in SmartStruxure WebStation

Product Line

SmartStruxure Solution

Environment

WebStation

Cause

Starting with SmartStruxure WebStation 1.6.0 there are HTML5 viewers available for both graphics and trends. However, the Java viewer is the default so the HTML5 viewer must be enabled.

Resolution

Note: As of WebStation version 1.6.0, the HTML5 viewers are still in beta and still have some compatibility issues.

To use the HTML5 viewers take the following steps:

1) Log into WebStation

2) On the upper right-hand side click on Settings and then check the Use HTML5 viewers option