How do I enable analog video on the Pelco Camera Tester Tool IPCT01?

Issue

Connect and Enable Analog Video on the IPCT01.

Product Line

Pelco Cameras

Environment

  • IPCT01 Pelco IP Camera Installation Tool

Cause

  • Installation and Configuration
  • Enable Analog Video Display

Resolution

Enable Analog Video

Users can view analog video through the BNC IN connector on top of the IPCT01. Connect the video cable to the BNC connector.

Power on the IPCT01. Click on The Analog Video Icon .

 

Video Displays

Related Topics:

How do I Wire and Configure PTZ (Pan, Tilt, and Zoom) control on the Pelco Camera Tester Tool IPCT01?