How do I Wire and Configure PTZ (Pan, Tilt, and Zoom) control on the Pelco Camera Tester Tool IPCT01?

Issue

Wire and configure the IPCT01 for PTZ control.

Product Line

Pelco Cameras

Environment

  •  IPCT01 Pelco IP Camera Installation Tool

Cause

  •  Installation and Configuration
  • Control Analog PTZ Cameras

Resolution

Wire Control Cables to the IPCT01

Conect wires to the TX+ and TX- terminals on the IPCT01. Connect other end maintaining polarity to the RX terminals on the camera.

Configure IPCT01 for Protocol (Language) and Communication Rate (Baud)

 Power on the IPCT01. Click on Setup Icon  from the Main Menu.

Click on the Analog Video Icon . Open the AV Dome  settings to configure the cameras PTZ properties.

Enable the RS485 Output; Select Protocol and baud rate.

Apply Changes

 

Related Topics:

How do I enable analog video on the Pelco Camera Tester Tool IPCT01