Is there a way to concatenate access events from two Personnel objects into one Personnel object?

Issue

Is there a way to concatenate access events from two Personnel objects into one Personnel object? 

Product Line

Andover Continuum

Environment

Continuum Cyberstation

Cause

A Personnel object had a history of events and was then mistakenly recreated as a duplicate object. The original object was disabled and new events have now been tied to the new duplicate Personnel resulting in events for the same person being spread across two Personnel objects.

Resolution

The Access events produced are linked to each individual Personnel object that created them. There is no way to transfer these events from one Personnel to another.