VideoXpert: How to add or remove Pelco cameras to a recorder.

Issue

Pelco cameras need to be assigned or removed from a VideoXpert recorder.

Product Line

Pelco Video Management

Environment

VideoXpert 1.8+
NSM5200 version 2.4.3 +

Cause

This document will be a baseline for customers to go off of.

Resolution

Note: Do not move cameras between 2 different storage devices; attempting to unassign a camera from a NSM5200 and adding it to an VXS will prevent you from accessing video stored on the previous recording platform.
 
Adding Pelco cameras to a VideoXpert recorder:
  1. Open a web browser to the VideoXpert Core and login with [Username: admin Password: your_specific_password].
  2. Click Storage select the NSM5200 then click Add or Remove Cameras.


     
  3. Select the required cameras on the right then click Add to Pool then click Done.



     

 

If the camera to be recorded does not appear in the list because it has been recorded on another storage server in the system, the "Only find Data Sources not assigned to *any* recorder" box must be unchecked so the camera will appear in the list:

 

 

Removing Pelco cameras from a VideoXpert recorder

  1. Open a web browser to the VideoXpert Core and login with [Username: admin Password: your_specific_password].
  2. Click Storage select the NSM5200 then click Add or Remove Cameras.
  3. Select the required cameras on the left then click Remove from Pool then click Done.