How do I find The EVO Series Oncam Grandeye Cameras on my network?

Issue

Discovering and Viewing EVO Cameras on the Network

Product Line

Pelco Cameras

Environment

  • EVO Series

Cause

  • Installation and Service
  • Camera has been addressed via DHCP; current assignment unknown.

Resolution

To discover the Evolution Series Cameras across a network, using the Oncam Global IP Configuration Tool.

Download the tool from Oncams website:  EVO Camera Configuration Tool

One can also find all of the Oncam Grandeye applications on Pelco.com on the Evolution 360 product pages.

 

Finding the Evolution 360-Degree cameras

The Oncam Grandeye Configuration Tool is similar in functionality to Pelco’s Device Utility

(DU2). The Oncam Grandeye Configuration Tool interface looks like:

It will display all of the Evolution 360-Degree cameras that it finds on the network.

 

To discover the Evolution Series Cameras across a network, using Endura Utilities.

Endura Utilities finds the cameras – either directly on a network, or under the UDI5000 that they are attached to. Not all of the Endura Utilities functionality has been integrated at this time.

Direct network cameras:

UDI5000 connected cameras:

From the “Systems Attributes” tab under non-Endura devices:

From the “Devices” tab under non-Endura devices:

From the “Devices” tab under the UDI5000:

 

Related Topics:

How to add and configure an Oncam Grandeye EVO-05 to a Digital Sentry (DSSRV) recorder.