Spectra Heavy Duty lower dome cage part number.

Issue

  • What is the Heavy Duty cage part number?
  • What is the lower dome cage part number on the Spectra Heavy Duty camera models?
  • The Spectra models have a cage on the botom of them; what is that part number?

Product Line

Pelco Cameras

Environment

  • LD53HDCPB-0
  • LD53HDCPB-1
  • SD4xx-HPx1 or SD4xx-HFx1 Spectra IV Heavy Duty

Cause

Lower cage to the lower dome of the Spectra Heavy Duty models has a part number reference that is difficult to find.

Resolution

The Spectra IV Heavy Duty lower dome cage part number is MF03-1040-036E.