Focus slider will go back to 50 when set to manual on IME/ IXE series

Issue

The focus slider will go to 50 when set to manual mode, even if it was set to a different position

Product Line

Pelco Cameras, Pelco Video Management

Environment

IME and IXE series when setting focus to manual

Cause

The slider will go to the middle of the setting when set to manual if using IE, this is a problem with IE settings

Resolution

Set this in Firefox and it will stay at the location it was set to before changed to manual focus