What is the battery part numbers on CM6800 series?

WARNING

ELECTROSTATIC DISCHARGE REQUIRED.
Discharge all static electricity from your person by touching metal prior to handling any hardware. Failure to do so may result in damage to devices.

NOTICE

DISCONTINUED PELCO PRODUCT.
This product has been discontinued. For further information please visit pelco.com/support/discontinued-products

Issue

What is the battery part numbers on CM6800 series?

Product Line

Pelco Matrix

Environment

  • CM6800-32X6
  • CM6800E-48X8

Cause

After power cycle the CM6800 has lost all cameras as well as configuration.

Resolution

  • Need to replaces the battery on CM6800:
  • There are two types of battery on CM6800
  • Soldering on battery part numbers ZH64-3053-1201
  • Removable battery part numbers BATLCCBR2330