How Do I Connect Power to the WCS1-4.

DANGER

HAZARD OF ELECTRIC SHOCK.
Remove all power from all devices before removing any covers or doors of the system. Disconnect the power at the device and at the power source.

NOTICE

COMPLEX PROCEDURE REQUIRED.
The resolution of this article has many complex steps that may result in unforeseen results if not performed correctly. If you are at all unfamiliar with the requirements, please contact Product Support Services for assistance.

Issue

What is the connection method for powring the WCS Series power supply.

Product Line

Pelco Transmission & Power

Environment

  • WCS1-4 Series
  • WCS4-20B Series

Cause

Installation and Service

Resolution

WARNING: The WCS1-4 does not have an on/off switch. Turn off power at the circuit breaker before wiring the power supply.

To install the input power wires to the WCS1-4 power supply, refer to Figure 4 and do the following:

1. Determine the size of the input wire needed.

2. Bring the wiring into the WCS1-4 through the conduit fitting.

3. Attach the neutral input power wire to the 100V, 120V, or 240V, NEUTRAL (COM) connection on the Primary Line Input connector strip. Attach the hot wire to the LINE connection on the same strip.

4. Attach the input ground wire to the No. 6 ground stud, located between the conduit holes, and tighten the wire with the nut and washer (supplied).

 

WCS1-4

WCS4-20B

 Related Topics:

Which Output Tap should be used when connecting to a WCS series power supply