What are the definitions for the enumerated value representing CTSTS (control status) for the Network 8000 MicroNet FLO2 controller?

Issue

What are the definitions for the enumerated value representing CTSTS (control status) for the Network 8000 MicroNet FLO2 controller?

Product Line

TAC I/A Series

Environment

IA Series G3 tacAsd driver

Cause

CTSTS is displayed as an enumerated value and the associated definition is not provide.

Resolution

The definitions for CTSTS (control status) are:

Hex - Decimal - Definition

0x00 0  CAL
0x01 1  UNOFF
0x02 2  WRMUP
0x03 3  REV
0x04 4  COOL
0x05 5  CLMX
0x06 6  CLMN
0x07 7  HEAT
0x08 8  HTMX
0x09 9  HTINT
0x0A 10  FOPN
0x0B 11  FCLS
0x0C 12  FMX
0x0D 13  FMN
0x0E 14  FFAN
0x0F 15  GFOPN
0x10 16  GFCLS
0x11 17  FGMX
0x12 18  GFMN
0x13 19  CALDP
0x14 20  DIAG