Can I install an IXE camera into the EHX*E series explosion proof camera enclosure

Issue

Can I install an IXE camera into the EHX*E series explosion proof camera enclosure

Product Line

Pelco Cameras

Environment

  • IXE
  • EHX6E Series
  • EHX8E Series
  • EHX6E-16

Cause

Enclosure to support IP camera within explosion rated housing.

Resolution

Yes. Only the Sarix IX series IP camera can be installed into the EHX6E, EHX8E or EHX6E-16 Series. Refer to page 2, section mechanical on the EHX*E Series Product Specification for maximum camera and lens size.