PMCL555NB VESA hole mounting dimensions vs PMCL555BL VESA.

Issue

Does the PMCL555NB use the same mounting as the PMCL555BL?

Product Line

Pelco Monitors

Environment

  • PMCL555NB
  • PMCL555BL
  • VESA
  • PMCLNBWMT
  • PMCLNBWMF
  • PMCLNBWMS

Cause

Existing monitor mount for previous Pelco monitor offer of PMCL555BL.

Resolution

The PMCL555NB uses the same Pelco mounting options of the PMCL555BL. The following mounts are designed to meet the monitor's different VESA hole dimensions:

  • PMCLNBWMT - Tilt wall mount
  • PMCLNBWMF - Flat wall mount
  • PMCLNBWMS - Swingout arm wall mount
     

Mounting Hole Dimensions

  • PMCL555BL - VESA 400 x 400 mm (15.7" x 15.7")
  • PMCL55NB  - VESA  600 x 400 mm ( 23.6" x 15.7")