Can a 24VDC external power supply be used with IEE20DN?

DANGER

HAZARD OF ELECTRIC SHOCK.
Remove all power from all devices before removing any covers or doors of the system. Disconnect the power at the device and at the power source.

Issue

Does IEE20DN support 24VDC external power supply?

Product Line

Pelco Cameras

Environment

  • IEE20DN-0
  • IEE20DN-1
  • IEE20DN-OCPO

Cause

24VDC power supply on site to power the IEE20DN

Resolution

IEE20DN can only be powered up with 24VAC or POE IEEE 802.3AF

 

Refer to IEE20DN spec Sheet Click here: