Issue
How do you change the default colors applied to the value of points placed on a graphics page?
Environment
I/NET Site
Cause
How does one change the default colors on a graphics page?
Resolution
Go into the graphic properties editor and choose one of the following:
Text Pen - Use this option to choose a default foreground color for point text. When you select this option the system displays the color dialog. You can choose a standard system color or you can define a custom color. This setting will be ignored if you have activated the Use Object Pen option described below.
Use Object Pen - When activated this option causes the default color for point values to be the color defined within the points font properties. Otherwise point values are displayed in the color you choose using the Text Pen option described above.
The Use Object Pen settings do not affect the color of text objects or markers. It also has no affect on points that have already been placed on the graphic page.