What PTZ Communication Protocols do NET5500 Series Video Encoders support?

Issue

PTZ Protocol Support information must be understood during design and implementation phase of equipment installation.

Product Line

Pelco Cameras, Pelco Video Management

Environment

  • NET5501
  • NET5504
  • NET5508
  • NET5516

Cause

Controlling devices (NET5500 Series in this case) must be able to communicate to Cameras using the appropriate PTZ Communication Protocol.

Resolution

NET5500 Series Encoders support the following PTZ Communications Protocols...

  • Coaxitron (15-bit)
  • Extended Coaxitron (32-bit)
  • RS-422/RS-485 (2/4-wire) using Pelco-D or Pelco-P protocols


See Also: