Why won't my DU2 scripts work with Spectra HD or enhanced cameras?

Issue

The DU2 scripts do not work on Spectra HD , enhanced cameras, or Pro series cameras

Product Line

Pelco Cameras, Pelco Video Management

Environment

when using DU2 scripts on Spectra HD, enhanced or pro cameras

Cause

The DU2 (device utility 2) scripts no longer work with the new 2.0 or newer series firmware ( due to Kernel changes), Also does not work with OEM/ ODM cameras such as Pro series , or Pelco Multi-Sensor Cameras.

Resolution

These will need new scripts either made by engineering or API commands may be used.