ENC5516 Power 1 and Power 2 LED's flash-blinking while link light is steady.

Issue

ENC5516 Power 1 and Power 2 LED's flash-blinking while link light is steady. Driver is detected in Windows Device Manager however ENC5516 displays no video.

Product Line

Pelco Video Management

Environment

  • ENC5516
  • DSSRV2
  • DSSRV - v7.7.309 or later

Cause

The ENC5516 will go into Voltage power protection mode, if power is unstable due to bad ENC5516 power supply or the power source not stable (ups, wall socket.)

Resolution

To get out Voltage protection mode,

  1. Power down DSSRV.
  2. Unplug power cord to ENC5516 for 10 minutes (this will allow the condenser to dischange.) 
  3. Plug power back to the ENC5516.
  4. Power up DSSRV and confirm if power LED is stable on ENC5516.

Note: If steps 1-4 do not work, replace ENC5516 Power supply.

  • ENC5516-PS: 12VDC power adapter.
  • ENC5516-PS-US: power adapter cable.


Related Articles:
How do I get a credit authorization?
How do I send in a Pelco product for repair services?