Is the SE7200 compatible with the SED-WIN-P-5045 wireless window switch ?

Issue

Datasheets indicate that the SE7200F5545P is compatible with the SED-WIN-P-5045 but changes in the switch are not being recognized by the SE7200. 

Product Line

SmartStruxure Lite

Environment

SE7200 wireless version

Cause

The SED-WIN wireless window switch was confirmed, as of the date of this article, as NOT compatible with the SE7200 controller model.

Compatibility will be available at a later date.

Resolution

If necessary, use the VT7200F5014P-2624 controller with the SED-WIN-P-5045. 

This controller has a Honeywell cover but it's functionally equivalent to the SE7200F5545P.  Just swap covers.