How do I adjust the white balance on the IS90-CHV22

Issue

How do I adjust the white balance on the IS90-CHV22

Product Line

Pelco Cameras

Environment

  • IS90-CH,DN,and C series

Cause

  • Video image washes out

Resolution

To adjust the IS90-DN, IS90-CH, or IS90-C models

 

Auto white balance (AWB) is enabled by default (OFF).

To manually set and lock the white balance:

  1. Set SW4-5 to OFF.
  2. Hold a white background in front of the lens until the video shows all white.
  3. While holding the background in place, set SW4-5 to ON. A blue blinking block appears on the video image for a few seconds. When the block changes to solid green, the manual white balance (MWB) process is complete.