How to generate Digital Sentry reports using DS ControlPoint.

Issue

How to generate Digital Sentry reports using DS ControlPoint.

Product Line

Pelco Video Management

Environment

  • Digital Sentry Series v4.2.2 (6.8.2.22) or later
  • DS ControlPoint v4.2.2 (6.8.2.22) or later

Cause

Report generation for camera usage report, activity report, zones/VAU report, configuration report and snap shot report.

Resolution

  1. Double-Click on the DS ControlPoint icon on the desktop or start menu.
     
  2. Click on Setup.

    DS ControlPoint Setup Icon
     
  3. In Setup click on the DigitalSENTRY Reports button.

    Setup Menu
     
  4. Select the location where you would like to save the report(s).

    Select Destination
     
  5. Select the system(s) that you would like to generate a report from then move them to the
    right side of the list by clicking the >> button.

    Systems Selection
     
  6. Click Next
     
  7. Select the type of report that you would like to generate as well as the date range
    for the report.

    Report Selection
     
  8. Click Next
     
  9. Click finalize to complete the report(s). The report(s) will be found in the location selected in step 4.

    Process Complete

 

NOTE: Reports cannot be run for DX Series products.