Where do I Connect Power on the IS90 Series camclosures?


Connect Power to The IS90 series cameras.

Product Line

Pelco Cameras


  • IS90 Series Camclosure


  • Installation and Service.


When connecting AC power to the device polarity is not an issue.

AC operation only: If you are wiring more than one Camclosure to the same transformer, connect one side of the transformer to the red wire on all units; connect the other side of the transformer to the black wire on all units.

NOTE: Failure to connect all AC powered units the same way will cause the cameras to be out of phase with each other and may produce a vertical roll when switching between cameras.