What is the tamper bit part number for ICS or IS series camera?

DANGER

HAZARD OF ELECTRIC SHOCK.
Remove all power from all devices before removing any covers or doors of the system. Disconnect the power at the device and at the power source.

Issue

What is the Tamper bit part number for ICS or IS series camera?

Product Line

Pelco Cameras

Environment

  • ICS100 series
  • ICS150 series
  • ICS200 series
  • IS110 series
  • IS150 series

Cause

Tamper bit required to open dome cover on ICS100

Resolution

Tamper bit part number: TS01-0205-2101.