Dataview and Dynaview

Issue

In Dataview and Dynaview, the am or pm is not shown when the time is after 10am to 12am or 10pm to 12pm when crosshairs is used on a graph

Product Line

Satchwell Sigma

Environment

Sigma 4.08

Cause

In Dataview and Dynaview, the am or pm is not shown after 10am or 10pm when crosshairs is used on a graph

Resolution

The workaround is to use the 24hr clock.

Goto Control Panel > Region and Language > Formats and change the Short Time and Long Time to a format that does not have 'tt'.