Power requirements for MX4004 series.

DANGER

HAZARD OF ELECTRIC SHOCK.
Remove all power from all devices before removing any covers or doors of the system. Disconnect the power at the device and at the power source.

Issue

Does MX4004CD take VAC/VDC input power?

Product Line

Pelco Matrix

Environment

  • MX4004CD
  • MX4004CD-X
  • MX4004CS

Cause

Power requirements to power up the MX4004 series genex.

Resolution

Part number for the wall block power supply:  

MX4004CD (USA MODEL 60HZ):  PS04-1800-0112 (120VAC, 12VDC)

MX4004CD-X (PAL MODEL 50HZ):  PS04-1503-9012 (90-264VAC,12VDC)