The FD Series Camclosure's Lower Dome has condensation or is fogged up.


The FD5,FD2, and FD1 series cameras have condensation build up around the lens during first installation. The condensation may or may not evaporate after camera operation.

Product Line

Pelco Cameras


  • FD5, FD2, FD1 Camclosure series


  • Moisture enters camera.


Avoid storing the unit in extremely humid, dusty, hot/cold environments where the operating temperature is outside the recommended range of -22F to 121F (-30C to +55C).

If camera is installed during a high humid day condensation may accumalate on the lower dome. 

The entire dome must be dried out a hair dryer works best.  Place dessicant inside the enclosure to absorb any moisure.


Related Topics:

The BU6 Lens fogs up or condenses after install