Does the Niagara R2 Transition Tool convert graphics?

Issue

Does the Niagara R2 Transition Tool convert graphics?

Product Line

TAC I/A Series, SmartStruxure Solution

Environment

Niagara R2

StruxureWare Building Operation

Cause

Product inquiry

Resolution

The tool does not convert graphical images.  It does convert bindings to inputs of a GxPage.  See the R2 Transition Guide (F-27835) for more details.  An excerpt from the guide follows:

3.4.3 GxPage

The TAC I/A Series R2 GxPage object is converted to a Building Operation Graphic object. The converted Graphic object contains a Dynamic Text object for each dynamic Gx object at the coordinates of the corresponding Gx object from the GxPage. The Dynamic Text objects in the Building Operation Graphic are named to match the corresponding Gx objects from the GxPage. Graphical images from the GxPage are not converted to the Building Operation database.

Bindings to inputs of the GxPage are converted to the Building Operation database as links to the corresponding Dynamic Text objects within the converted Graphic.