How do you enable the Alarm Export feature on DS control point.


Alarm Export icon is missing.

Product Line

Pelco Video Management


  • DS Control Point
  • DSSRV2
  • DS


No "Alarm export path" has been enter in DS Control Point.



  1. Open DS Control Point.
  2. Connect to Digital sentry system.
  3. Select "Setup" Icon
  4. Select "Application Settings" menu..
  5. Select the "Export" tab for the Export setting menu.
  6. Select the Alarm export path by clicking on the Browse Button.
  7. Press OK when alarm export path has been selected.
  8. Test by going into the alarm page and right click on image
  9. Select "Alarm Export" and this will export a html report to folder.