How to Undock a display in DS ControlPoint.

Issue

Unable to undock a display in DS ControlPoint to display different cameras on two different monitors.

Product Line

Pelco Video Management

Environment

  • DSSRV
  • DSSRV2
  • DSNVS
  • DS ControlPoint

Cause

  1. Server / Application operation assistance.
  2. Undock icon is not available (not showing).

Resolution

To Undock a configured display:

  1. First select the view pane for the number of cameras to be displayed.
     
  2. Drag the selected cameras into the desired view pane.
     
  3. Click the Undock icon (blue arrow pointing up) located next to the Help icon.
     
  4. Verify the display is now undock.
     
  5. Drag the new undocked display to the second monitor.
     

NOTE: This will also work for Groups that are already configured in DSCP.