Issue
Client Button Feature for Equalization
Environment
I/NET site
Cause
Is there a button available to users who are utilizing the Equalization Feature of I/NET?
Resolution
There is a new button available to users who are utilizing the Equalization Feature of I/NET. This button allows the user to see when the Clients were contacted last by the File Master and makes Trouble shooting easier.
The following shows how it should be set up and used:
- In the I/O Configuration, open the active profile (the one being used for Equalization on the File Master).
- Click on the Equalization File Master check box.
- Once Equalization has been set up and the Clients are on line, follow step 1 again.
- Click on the Clients Button, which is now active, a list of the Clients will show up.
- The user can now see the last time a Client was polled and it can be dropped by selecting it and clicking Drop.