How to Reset IBP Series camera.

Issue

Unknown IP Address

Product Line

Pelco Cameras

Environment

Sarix IBP Series Environmental Bullet Cameras

Cause

Reset the camera

Resolution

1. Loose the two screws and remove the metal cover then appears the interor buttons and inlets as the figure shows below.
2. Disconnect the power or unplug the cable from the POE Injector or POE switch
3. Hold down the Default Button to reset the ip address before reconnecting the power
4. Keep holding down the Default Button for 15 seconds.
5. Try to ping the camera at the default IP Address:  192.168.0.20

Note: Click HERE for IBP Series Installation Manuals