How to reset the Spectra Professional to factory default


Factoery Default the Spectra Pro

Product Line

Pelco Cameras


  • Spectra Professional Series
  • P1220


  • Unable to access camera web page.
  • Unable to ping IP camera.


Remove the dome bubble.  While the Camera is powered and linked to a network; press the Default Button for 5 seconds to restore the camera back to the factory default settings. There is not any indication of progress during IP assignment.  May take up to 10 minutes to assign an IP address.

Default IP: