Is it possible to specify the Subnet/node address for a Lon device?

Issue

In for example TAC Vista it was possible to specify the subnet/node address when adding a Lon device, is it possible to do this in any way in StruxureWare Building Operation(SBO)?

Product Line

SmartStruxure Solution

Environment

StruxureWare Building Operation version 1.6.1 and erlier.

Cause

No in version 1.6.1 this is not possible.

Resolution

The plan is to add this functionality to SBO version 1.7.
So hopefully this functionality is added to version 1.7 if implementation and testing goes well.