Issue
AVI files in I/NET Seven
Environment
I/NET Site
Cause
Are AVI files in I/NET Seven supported?
Resolution
While the AVI file is not an officially supported file format for use in graphic pages in I/NET Seven a limited functionality does exist.
The requirements for the AVI file that we have found is that the file must be an uncompressed AVI file and the smallest size file must be 40x40 pixels.
Be aware that when the point you have linked to this AVI file turns off it will not always return to the initial image of the AVI file. Rather the AVI file will stop where ever it was in the sequence when the point value changed. Because of this it is also recommended that you use the AVI file for the on state and a still image for the off state to maintain consistency.