I/NET fails to run as a Service

Issue

I/NET will run in application mode, but will quickly shut down when in service mode

Product Line

TAC I/NET

Environment

I/NET Configuration Profile

I/NET

I/O Server

Cause

The I/O Server can be configure to auto shutdown whenever the I/NET Workstation application is closed. If this setting is used, the service will stop whenever I/NET Workstation is closed as well.

Resolution

  1. Open the I/NET Configuration application. [Start>All Programs>I/NET>INET Config
  2. Click on the Radial button so that I/O Server is maintained when no clients are present. Do NOT use the shutdown option when using I/NET as a service