When using the TAC Vista Smartstruxere Interface, it necesary to configure any DCOM or firewall settings when you run TAC Vista and Smartstuxure or differnet computers?

Issue

  • When using the Smartstruxere Interface,  it necessary to  configure any DCOM or firewall settings  when you run TAC Vista and Smartstuxure or different computers
  • What protocol is used for communication between the Smartstruxure interface for TAC Vista and the ES

Product Line

TAC Vista, SmartStruxure Solution

Environment

TAC Vista server

TAC Vista Smartstruxure Interface

Smartstruxure enterprice server

Cause

Communication issues between interface and SBO

Resolution

Only HTTP/HTTPS are used.

You can conifugute the interface to use only one of the protocolls.

You can also configure the what ports to use