Can an EE500 database be imported into a SM5000/SM5200?

Issue

Customer is upgrading from an EnduraXpress EE500 to an Endura 2.0 system

Product Line

Pelco Video Management

Environment

  • EnduraXpress
  • EE500
  • SM5200
  • SM5000

Cause

Upgrade

Resolution

Importing the EnduraXpress (EE500) database to an SM5000 or SM5200 is not supported. The databases are significantly different.