Spectra Pro HD VPTZ must use POE+ to work properly.

Issue

The Spectra Pro VPTZ needs to use POE+ to be powered on the indoor cameras. This is for both the regular operation of the camera and the fans.

Product Line

Pelco Cameras, Pelco Video Management

Environment

Spectra Pro VPTZ when used indoors

Cause

The Spectra Pro VPTZ needs POE+ to power the camera functions,

Resolution

Power the indoor unit with POE+ and if using an outdoor environmental it is best to use 24 VAC at 50 VA