Getting an Invalid status code: 401 Access Denied error when doing a Save Runtime DB of the localhost or a Get to save a remote UNC station to the localhost.

Issue

Getting an "Invalid status code: 401 Access Denied" error when doing a “Save Runtime DB” of the localhost or a “Get” to save a remote UNC station to the localhost.

The errors read: 

Error when doing a “Save Runtime DB” of localhost station: 
tridium.nre.net.HttpException: Invalid status code: 401 (Access denied)
           at tridium.ui.admintool.DbAdminConfigPanel.doRemoteBackup(DbAdminConfigPanel.java:1100)
           at tridium.ui.admintool.DbAdminConfigPanel$Worker.run(DbAdminConfigPanel.java:1224)

Error when doing a “Get” of a remote UNC station:
           java.io.FileNotFoundException: c:\niagara\r2.301.535\stations\anystation\config.sns (Access is denied)
           at java.io.FileOutputStream.open(Native Method)
           at java.io.FileOutputStream.(Unknown Source)
           at java.io.FileOutputStream.(Unknown Source)
           at tridium.ui.admintool.DbAdminConfigPanel.doOnlineGet(DbAdminConfigPanel.java:848)
           at tridium.ui.admintool.DbAdminConfigPanel.doGet(DbAdminConfigPanel.java:764)
           at tridium.ui.admintool.DbAdminConfigPanel$Worker.run(DbAdminConfigPanel.java:1216)
 

Product Line

TAC I/A Series

Environment

WorkPlace Pro, ES, UNC

Cause

Either the username or password, or both, being used are invalid. A valid username and password must be entered to perform a “Save Runtime DB” of the locahost, or a “Get” to save a remote station to the localhost.

Resolution

Use a valid station username and password to perform these functions on the locahost.