Where do I land the Video Cable on a Spectra PTZ Camera


What are my Video connection options for the Spectra Series of Cameras

Product Line

Pelco Cameras


  • Spectra II, Spectra III, and Spectra Iv Series
  • SD5, SD53,SD4


Installation connections for video cabling.


Coaxial Cable RG59, RG6, and RG 11

Connect coax  to the BNC connector on the swivel-down circuit board inside the camera housing:

Spectra II Spectra III

When connecting the video cable, the Spectra IV provides a coaxial and a CAT5 UTP connection:


 Related Topics:

Where do I land the data wires on the Spectra back box for RS422 two wire Pin Out and control