What are the recommended tolerances and specifications of the terminal block in the DF5 series dome enclosure?

Issue

Specific parameters and tolerances needed for field installation accountability.

Product Line

Pelco Cameras

Environment

DF5 Series DomePak

Cause

Documented reference required for field service installation requirements.

Resolution

The specific parameter ratings for the TB06-1411-4110 terminal block inside the DF5 fixed dome enclosure are:

Rated voltage: 250 V

Rated current: 17.5 A

Maximum wire size: 1.5 mm

Test voltage: 2.0 kV

Rated torque with M2.6 screw size: 0.4 Nm