Which PTZ protocols does DX4104 series DVR support?

Issue

DX4104 is being used with non-Pelco brand PTZ cameras.

Product Line

Pelco Video Management

Environment

DX4104
Non-Pelco brand PTZ camera

Cause

Installer/integrator needs to know with which PTZ cameras DX4104 is compatible.

Resolution

Please refer to the following table of PTZ protocols and functions that DX4104 supports:

Protocol Name Pan/Tilt Zoom Focus Iris Preset Tour Setup
LG_MULTIX Yes Yes Yes Yes Yes Yes Yes
LG_SD168 Yes Yes Yes Yes Yes Yes Yes
PELCO_D Yes Yes Yes Yes Yes Yes Yes
PELCO_P Yes Yes Yes Yes Yes Yes Yes
GANZ_DSCP Yes Yes Yes Yes Yes Yes Yes
GANZ_P360V1 Yes Yes Yes Yes Yes Yes No
KALATEL_CYBERDOME Yes Yes Yes Yes Yes Yes No
PANASONIC_CS850 Yes Yes Yes Yes Yes Yes Yes
SAMSUNG_SCC Yes Yes Yes Yes Yes Yes Yes
LG_ZOOM No Yes Yes Yes No No Yes
LPT_A100L Yes No No No No No No

 

For any camera brands that are not listed, a third-party PTZ protocol converter may be used, such as Sennetech Video & Control Interface Products:

http://sennetech.net