IAC400 and IAC600, a digital output cannot be forced to a different value

Issue

IAC400 and IAC600, a digital output cannot be forced to a different value

Product Line

Satchwell MicroNet, SmartStruxure Solution

Environment

IAC400

IAC600

SBO

Cause

When an IAC400 or IAC600 is imported into SBO using the Micronet interface, on a digital output, the output cannot be forced to another value.

Resolution

In Visisat, create the SBO export file.

Before using the 'Data Import' into the Micronet Interface in SBO, locate and open the export xml file with a suitable program e.g. notepad++.

Locate the respective controller's 'Digital Output Overide State' part and on the line <P1="IsNonVolatile...." (Note, if opened in another application e.g. Internet Explorer, the word order may be different!)

 change the Value= "1" to Value="0"

 

Note: IAC420s are unaffected