When Exporting Bookmarked Video on a DX8100 using Axis Cameras, The Time and Dates are Incorrect.

Issue

Start times and end times displayed on bookmarked video are in correct for exporting.

Product Line

Pelco Video Management

Environment

  • DX8100 Series 2.0 and above
  • All Axis Cameras

Cause

The DX8100 IP camera driver doeasn't support bookmarking correctly.

Resolution

The DX8100 is end of life and will have no further development.

Workaround

When exporting bookmarked video, edit the field that displays the incorrect information.

Double click in the field and edit.