ES Database Size

Issue

ES Database has grown to several gigabyte

Product Line

SmartStruxure Solution

Environment

StruxureWare Building Operation site with Enterprise Server

Cause

ES Database size can grow quite large when the ES crashes often. Open Software Administrator and find the location of the ES db folder. Below are two screen shots of the Logs and Crash Information folders. As you can see, these dump files can increase the size of the database.

Resolution

Once the reason for the Enterprise Server crash is resolved, these files can be either be deleted or, preferably be moved to another storage/drive location.